New at Mouser: Würth Elektronik’s WSEN-ISDS 6-Axis Inertial Measurement Unit for Drone and Robotic Applications

Annonce de nouveaux produits

Retrouvez-nous sur


August 23, 2023Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now shipping the WSEN-ISDS 6-axis inertial measurement unit (IMU) from Würth Elektronik. The WSEN-ISDS IMU is a 16-bit digital ultra-low power and high-performance sensor featuring a 3-axis accelerometer and a 3-axis s gyroscope, with selectable measuring ranges and data rates. This versatile motion sensor facilitates integration, with output and processed data pre-calibrated, for application-specific functionalities like localization and navigation for robotics, drones, automation, industrial tools, machines, antenna, platform stabilization and Industrial IoT (IIoT) devices.

The Würth Elektronik WSEN-ISDS 6-axis IMU, available from Mouser Electronics, includes free-fall, wake-up, tap, activity, motion, tilt, and orientation detection functionalities, featuring linear and angular acceleration measurement, extending from single-event registration to high-frequency continuous vibration monitoring. User-selectable acceleration measurement ranges of ±2g, ±4g, ±8g, ±16g and an angular rate range of ±125 dps, ±250 dps, ±500 dps, ±1000 dps, ±2000 degrees per second enhance design versatility. Selectable data rates up to 937 Hz for the gyroscope and up to 1400 Hz for the accelerometer, with a built-in FIFO buffer to store the output data rate up to 6.6kHz, further enhancing flexibility in the design process. The WSEN-ISDS sensor features ultra-small dimensions (2.5 mm × 3.0 mm × 0.86 mm), an embedded temperature sensor and is available in a land grid array (LGA) package.

The Würth Elektronik WSEN-EVAL evaluation board provides the opportunity to verify the sensor performance and develop fast prototyping using an extension board. This evaluation board is designed to be used with either the Sensor Shield for Arduino (2501000101291) or the Sensor FeatherWing (2501000201291). The WSEN-EVAL evaluation board can also be mounted on a breadboard using through-hole pin header connections.

To learn more about the WSEN-ISDS 6-axis IMU, visit https://www.mouser.com/new/wurth-elektronik/wurth-6-axis-imus/.

To learn more about WSEN-EVAL evaluation board, visit https://www.mouser.com/new/wurth-elektronik/wurth-6-axis-imu-eval-board/.

The WSEN-ISDS IMU and WSEN-EVAL evaluation board were recently featured in the July 11 edition of Mouser’s “New Tech Tuesday” blog, Precision Agriculture Takes Flight: Enhancing Farming Efficiency with Drone Technology.

 

Distributeur mondial agréé, Mouser dispose de la plus vaste sélection au monde de semi-conducteurs et composants électroniques à la pointe de la technologie, en stock et prêts à être expédiés. Les clients Mouser peuvent compter sur des produits d’origine entièrement certifiés dont la traçabilité de chacun de ses partenaires de fabrication est garantie. Afin d’accélérer le processus de conception des clients, le site Internet de Mouser propose une vaste bibliothèque comportant des ressources techniques, dont un centre de ressources techniques, ainsi que des fiches techniques, des conceptions de référence propres à des fournisseurs, des notes d’application, des informations sur des conceptions techniques, des outils d’ingénierie et bien d’autres informations pratiques.

À propos de Mouser

2026 - Mouser Electronics est un distributeur agréé de semi-conducteurs et de composants électroniques, spécialisé dans le lancement de nouveaux produits de ses partenaires de premier plan. Le site Internet du distributeur, Mouser.fr, est disponible en plusieurs langues et dans plusieurs devises, et propose plus de 6,8 millions de produits de plus de 1 200 marques de fabricants. Mouser dispose de 28 sites répartis dans le monde entier afin d’offrir à ses clients un service d’excellence dans la langue, la devise et le fuseau horaire du pays respectif. Le distributeur expédie ses produits à plus de 650 000 clients dans plus de 223 pays/territoires depuis son centre logistique de 93 000 m² de Dallas (Texas). Pour plus d'informations, rendez-vous sur https://www.mouser.fr.

À propos Würth Elektronik

2026 - Würth Elektronik eiSos GmbH & Co. KG est un fabricant de composants électroniques et électromécaniques pour l'industrie électronique. Les sites de production en Europe, en Asie et en Amérique du Nord approvisionnent un nombre croissant de clients dans le monde entier. Le programme produit comprend les composants CEM, les inducteurs, les transformateurs, les composants HF, les varistances, les condensateurs, les modules d'alimentation, les LED, les connecteurs de fiches, les éléments d'alimentation, les bobines d'alimentation sans fil, les commutateurs, la technologie de connexion et les supports de fusibles. Würth Elektronik eiSos GmbH & Co. KG, avec ses sociétés affiliées spécialisées, forme le groupe Würth Elektronik eiSos.

Marques déposées

Mouser et Mouser Electronics sont des marques déposées de Mouser Electronics, Inc. Tous les autres produits, logos et noms de société cités dans le présent document, peuvent être des marques commerciales de leurs propriétaires respectifs.

Pour tout complément d'information, contactez :
Kevin Hess, Mouser Electronics
Vice-président senior responsable du marketing
+1 (817) 804-3833
Pour les questions liées à la presse, contactez :
Kelly DeGarmo, Mouser Electronics
Responsable de la communication institutionnelle et des relations avec les médias
+1 (817) 804-7764