Mouser Electronics Expands Antenna Range with New Embedded, Flexible and External Wi-Fi 6E Solutions

Annonce de nouveaux produits

Retrouvez-nous sur


Spotlight: Wi-Fi 6E Antenna Solutions

January 9, 2024Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, broadens its range of antennas designed for high-speed Wi-Fi 6E communication.

The introduction of IEEE's 802.11ax wireless standard brought forth several technical initiatives aimed at advancing connectivity for the next generation of devices. One key addition was the inclusion of Wi-Fi 6E, enabling Wi-Fi communication on the 6GHz spectrum for the first time. By operating at frequencies above the existing 2.4 and 5 GHz networks, Wi-Fi 6E enables better optimization, less interference, and lower latency. Security is also enhanced, as Wi-Fi Protected Access 3 (WPA3) certification is mandatory for all Wi-Fi 6E devices. Since its introduction in 2020, the deployment of Wi-Fi 6E has expanded to a diverse range of industrial and consumer locations, including offices, manufacturing facilities, clinical environments, and residential areas. Consequently, supporting Wi-Fi 6E has become essential for the latest high-performance wireless devices.

Mouser stocks a wide range of antenna designs needed to fulfill the diverse technical requirements of Wi-Fi 6E devices. Some of the newly added solutions include:

  • The UAM Wi-Fi® 6E/Wi-Fi 7 Embedded Antennas from Linx Technologies / TE Connectivity are an innovative range of omnidirectional tri-band antennas designed for the latest Wi-Fi 6E devices. As an externally mounted solution, they can be easily attached to a metal chassis using the unique snap-in feature, removing the need for fixings, allowing for unambiguous mounting direction, and increasing assembly speed. Alongside Wi-Fi 6E functionality, they allow for wireless Bluetooth® and ZigBee communication, as well as supporting future Wi-Fi 7 networks. The RoHS-compliant range includes multiple cable lengths, with MHF4l and MHF termination available, and is suitable for a wide range of indoor applications.
  • The Tri-band Wi-Fi 6E Flexible Printed Antenna from Abracon provides high-performance communications in low-profile and easy-to-integrate packaging. The omnidirectional tri-band operation provides high performance across 2400MHz to 7125MHz frequencies, covering vital 2.4 GHz, 5 GHz, and 6 GHz bands. The antenna helps to enhance the range of Wi-Fi signals, providing dependable and high-speed connectivity in congested public spaces and complex industrial settings. In conjunction with Wi-Fi 4/5,6/6E and 7 connectivity, it is also ideal for devices using Bluetooth, ZigBee, Thread, and Matter protocols. System assembly is straightforward, with the flexible design allowing for quick adhesive mounting even along contours. The antenna is suitable for a variety of routers and network devices, as well as home automation and IoT sensors.
  • Kyocera AVX's range of antennas includes solutions designed to suit a variety of Wi-Fi-connected applications. The FR4-based WXP3015W08 antenna features an embedded Wi-Fi dipole design and delivers high-performance connectivity and signal sensitivity in miniaturized packaging. It consumes minimal space and can easily be mounted through simple adhesion. For Wi-Fi 6E connections, it features a peak gain of 5.90dBi and an average efficiency of 60%, ensuring a strong connection. It is also suitable for previous iterations of Wi-Fi, as well as Bluetooth, BLE, and ZIGBEE protocols. Kyocera's RoHS-compliant AVX range also includes stamped metal and flexible printed circuit Wi-Fi 6E antennas, which use its patented isolated magnetic dipole (IMD) technology, as well as several cable lengths and termination options.

In 2023, Mouser launched more than 66,000 part numbers ready for shipment, including over 8,000 in the fourth quarter. To see more new innovative products, visit https://info.mouser.com/new_products/.

 

Distributeur mondial agréé, Mouser dispose de la plus vaste sélection au monde de semi-conducteurs et composants électroniques à la pointe de la technologie, en stock et prêts à être expédiés. Les clients Mouser peuvent compter sur des produits d’origine entièrement certifiés dont la traçabilité de chacun de ses partenaires de fabrication est garantie. Afin d’accélérer le processus de conception des clients, le site Internet de Mouser propose une vaste bibliothèque comportant des ressources techniques, dont un centre de ressources techniques, ainsi que des fiches techniques, des conceptions de référence propres à des fournisseurs, des notes d’application, des informations sur des conceptions techniques, des outils d’ingénierie et bien d’autres informations pratiques.

À propos de Mouser

2026 - Mouser Electronics est un distributeur agréé de semi-conducteurs et de composants électroniques, spécialisé dans le lancement de nouveaux produits de ses partenaires de premier plan. Le site Internet du distributeur, Mouser.fr, est disponible en plusieurs langues et dans plusieurs devises, et propose plus de 6,8 millions de produits de plus de 1 200 marques de fabricants. Mouser dispose de 28 sites répartis dans le monde entier afin d’offrir à ses clients un service d’excellence dans la langue, la devise et le fuseau horaire du pays respectif. Le distributeur expédie ses produits à plus de 650 000 clients dans plus de 223 pays/territoires depuis son centre logistique de 93 000 m² de Dallas (Texas). Pour plus d'informations, rendez-vous sur https://www.mouser.fr.

Marques déposées

Mouser et Mouser Electronics sont des marques déposées de Mouser Electronics, Inc. Tous les autres produits, logos et noms de société cités dans le présent document, peuvent être des marques commerciales de leurs propriétaires respectifs.

Pour tout complément d'information, contactez :
Kevin Hess, Mouser Electronics
Vice-président senior responsable du marketing
+1 (817) 804-3833
Pour les questions liées à la presse, contactez :
Kelly DeGarmo, Mouser Electronics
Responsable de la communication institutionnelle et des relations avec les médias
+1 (817) 804-7764