Mouser Electronics, onsemi, and Würth Elektronik Partner to Provide Solutions for Next-Generation Solar and Storage Systems
November 18, 2024 – Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, has partnered with onsemi and Würth Elektronik to address the growing solar inverter market.
The growth of the global inverter market is primarily driven by the easy installation of micro and string inverters, as well as an increase in investment toward renewable power infrastructure construction. Significant investment in rural electrification and the renewable energy sector is expected to create lucrative opportunities for existing and emerging players in the market.
onsemi's Silicon Carbide (SiC) solutions address the needs for the highest levels of efficiency, reliability, and safety while their boost and inverter power integrated modules (PIMs) anchor the grid-interface electronics. Würth Elektronik's gate drivers, sensing control, and peripheral power products complete the system.
The onsemi NXH40B120MNQ1 is an EliteSiC PIM containing a dual full SiC boost stage consisting of three 40mohm/1200V SiC MOSFETs and three 40A/1200V SiC diodes. The module features low reverse recovery, fast-switching SiC diodes, a low inductive layout, solderable pins, and an integrated thermistor. This SiC MOSFET module is suitable for solar inverters and uninterruptable power supplies.
Using the novel field stop 7th generation technology and the Gen7 Diode in a TO247 3−lead package, the onsemi FGY140T120SWD 1200V 140A Fast Discrete IGBT offers the optimum performance with low switching and conduction losses for high-efficiency operations in applications like Solar, UPS, and energy storage systems.
The Würth Elektronik WE-AGDT high-power auxiliary gate drive transformers feature unipolar and bipolar outputs, making them suitable for powering state-of-the-art SiC MOSFET gate drivers up to 6W of power as well as IGBT and power MOSFETs.
The WE-CSTLF current sense transformers, also from Würth Elektronik, are specifically designed for low frequencies, catering to 50Hz/60Hz applications such as power lines. The WE-CSTLF series utilizes a laminated core material that effectively handles low frequencies, ensuring optimal performance and durability even in challenging operating conditions.
To learn more about onsemi and Würth Elektronik's solar inverter solutions, visit https://www.mouser.com/new/onsemi/onsemi-wurth-solar-inverter-solutions/.
Distributeur mondial agréé, Mouser dispose de la plus vaste sélection au monde de semi-conducteurs et composants électroniques à la pointe de la technologie, en stock et prêts à être expédiés. Les clients Mouser peuvent compter sur des produits d’origine entièrement certifiés dont la traçabilité de chacun de ses partenaires de fabrication est garantie. Afin d’accélérer le processus de conception des clients, le site Internet de Mouser propose une vaste bibliothèque comportant des ressources techniques, dont un centre de ressources techniques, ainsi que des fiches techniques, des conceptions de référence propres à des fournisseurs, des notes d’application, des informations sur des conceptions techniques, des outils d’ingénierie et bien d’autres informations pratiques.
2026 - Mouser Electronics est un distributeur agréé de semi-conducteurs et de composants électroniques, spécialisé dans le lancement de nouveaux produits de ses partenaires de premier plan. Le site Internet du distributeur, Mouser.fr, est disponible en plusieurs langues et dans plusieurs devises, et propose plus de 6,8 millions de produits de plus de 1 200 marques de fabricants. Mouser dispose de 28 sites répartis dans le monde entier afin d’offrir à ses clients un service d’excellence dans la langue, la devise et le fuseau horaire du pays respectif. Le distributeur expédie ses produits à plus de 650 000 clients dans plus de 223 pays/territoires depuis son centre logistique de 93 000 m² de Dallas (Texas). Pour plus d'informations, rendez-vous sur https://www.mouser.fr.
2026 - onsemi aide à construire un avenir meilleur en stimulant des innovations révolutionnaires. Axée sur les marchés finaux industriels et automobiles, cette société accélère l'évolution des méga-tendances telles que l'électrification et la sécurité des véhicules, l'automatisation industrielle, les réseaux d'énergie durables et les infrastructures 5G et cloud. Onsemi propose une palette de produits novateurs et élabore des technologies d’alimentation et de détection intelligentes qui permettent de relever des défis complexes. L’objectif visé est un monde plus propre, plus sûr et plus intelligent. onsemi exploite des programmes de chaîne d'approvisionnement et de qualité fiables et réactifs, ainsi que des programmes ESG solides, et dispose d'un réseau mondial d'installations de fabrication, de bureaux de vente et de marketing, de même que des centres d'ingénierie sur ses marchés clés.
2026 - Würth Elektronik eiSos GmbH & Co. KG est un fabricant de composants électroniques et électromécaniques pour l'industrie électronique. Les sites de production en Europe, en Asie et en Amérique du Nord approvisionnent un nombre croissant de clients dans le monde entier. Le programme produit comprend les composants CEM, les inducteurs, les transformateurs, les composants HF, les varistances, les condensateurs, les modules d'alimentation, les LED, les connecteurs de fiches, les éléments d'alimentation, les bobines d'alimentation sans fil, les commutateurs, la technologie de connexion et les supports de fusibles. Würth Elektronik eiSos GmbH & Co. KG, avec ses sociétés affiliées spécialisées, forme le groupe Würth Elektronik eiSos.
Mouser et Mouser Electronics sont des marques déposées de Mouser Electronics, Inc. Tous les autres produits, logos et noms de société cités dans le présent document, peuvent être des marques commerciales de leurs propriétaires respectifs.