Now at Mouser: Infineon Technologies' NBT2000 OPTIGA NBT NFC Bridge Tag for Contactless Authentication of IoT Devices

Annonce de nouveaux produits

Retrouvez-nous sur


Learn more about the NBT2000 OPTIGA NBT NFC Bridge tag
Learn more about the NBT2000 OPTIGA NBT NFC Bridge tag

September 8, 2025Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the NBT2000 OPTIGA™ NBT NFC Bridge tag from Infineon Technologies. The NBT2000 is a ready-to-use bridge tag for single-tap authentication and secured configuration of IoT devices. The NBT2000 supports a range of applications, including product activation, device pairing, fault diagnostics, shared mobility solutions, and smart home devices.

The Infineon Technologies NBT2000 OPTIGA NBT NFC bridge tag, now available at Mouser, features a contactless passive Near Field Communication (NFC) interface and an Inter-Integrated Circuit (I2C) target interface for high-performance NFC-to-I2C communication. The NBT2000 bridge tag is NFC Forum Type 4 certified and includes an 8KB file system with file-based password protection, one-way authentication using ECDSA asymmetric cryptography, and symmetric AES-128-CMAC-based cryptography. OPTIGA Authenticate NBT ensures ultra-fast data exchange, even at high volumes.

The NBT2000 offers three operation modes: authentication, pass-through, and asynchronous data transfer. The bridge tag's power supply options include an external NFC field or an external power supply (VCC or GND). The NBT2000 bridge tag operates from -40°C to +85°C and has a +105°C maximum ambient temperature rating for I2C communication. The bridge tag can be used for applications such as secured configuration of electronic devices without a display, activation of shared mobility vehicles, and data logging on patient health monitors.

Infineon Technologies offers two development tools for the NBT2000 bridge tag: the OPTIGA™ Authenticate NBT development kit and the OPTIGA™ Authenticate NBT development shield, both available from Mouser. Both development tools include pre-tuned antennas, a comprehensive software package, and an NFC-I2C bridge tag. The development kit is an "all-you-need" bundle, where the development shield is designed to be used with an Arduino UNO-compatible microcontroller board.

To learn more, visit https://www.mouser.com/new/infineon/infineon-nbt2000-optiga-nfc-bridge-tag/

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

Distributeur mondial agréé, Mouser dispose de la plus vaste sélection au monde de semi-conducteurs et composants électroniques à la pointe de la technologie, en stock et prêts à être expédiés. Les clients Mouser peuvent compter sur des produits d’origine entièrement certifiés dont la traçabilité de chacun de ses partenaires de fabrication est garantie. Afin d’accélérer le processus de conception des clients, le site Internet de Mouser propose une vaste bibliothèque comportant des ressources techniques, dont un centre de ressources techniques, ainsi que des fiches techniques, des conceptions de référence propres à des fournisseurs, des notes d’application, des informations sur des conceptions techniques, des outils d’ingénierie et bien d’autres informations pratiques.

À propos de Mouser

2026 - Mouser Electronics est un distributeur agréé de semi-conducteurs et de composants électroniques, spécialisé dans le lancement de nouveaux produits de ses partenaires de premier plan. Le site Internet du distributeur, Mouser.fr, est disponible en plusieurs langues et dans plusieurs devises, et propose plus de 6,8 millions de produits de plus de 1 200 marques de fabricants. Mouser dispose de 28 sites répartis dans le monde entier afin d’offrir à ses clients un service d’excellence dans la langue, la devise et le fuseau horaire du pays respectif. Le distributeur expédie ses produits à plus de 650 000 clients dans plus de 223 pays/territoires depuis son centre logistique de 93 000 m² de Dallas (Texas). Pour plus d'informations, rendez-vous sur https://www.mouser.fr.

À propos de Infineon Technologies

2026 - Infineon Technologies est un concepteur, fabricant et fournisseur mondial de premier plan d’une large gamme de semi-conducteurs utilisés dans diverses applications microélectroniques. Le portefeuille de produits Infineon se compose de produits logiques, notamment de circuits intégrés numériques, à signaux mixtes et analogiques, ainsi que de produits semi-conducteurs discrets.

Marques déposées

Mouser et Mouser Electronics sont des marques déposées de Mouser Electronics, Inc. Tous les autres produits, logos et noms de société cités dans le présent document, peuvent être des marques commerciales de leurs propriétaires respectifs.

Pour tout complément d'information, contactez :
Kevin Hess, Mouser Electronics
Vice-président senior responsable du marketing
+1 (817) 804-3833
Pour les questions liées à la presse, contactez :
Kelly DeGarmo, Mouser Electronics
Responsable de la communication institutionnelle et des relations avec les médias
+1 (817) 804-7764