Ezurio's Nitrogen8M Mini SMARC Customizable SOM Delivers Edge Processing for HMI and Industrial Apps, Now at Mouser

Annonce de nouveaux produits

Retrouvez-nous sur


May 6, 2023Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now stocking the Nitrogen8M Mini SMARC from Ezurio (formerly Laird Connectivity). As part of the company's comprehensive system-on-module (SOM) portfolio, the Nitrogen8M Mini SMARC® conforms to the SMARC® 2.1.1 industry standard, offering global certification, a standard form factor, multiple software options, a proven security architecture, accelerated video/audio, long-term software support and security fixes that are well-suited for industrial IoT (IIoT) and HMI applications. This powerful and customizable solution enables heterogeneous multiprocessing, offers numerous interfaces and presents a smooth migration path to future long-term support and design-ins using the latest processors and wireless options as new Ezurio SMARC® SOMs are released.

The Ezurio Nitrogen8M Mini SMARC, available from Mouser Electronics, is a robust SOM powered by NXP's first-in-class i.MX 8M Mini applications processor, with optional Sona™ Wi-Fi 6/6E and Bluetooth® 5.3/5.4 wireless modules based on leading Infineon and NXP solutions, and the NXP PF8121 power management IC. The SOM provides high-performance LPDDR4 RAM / eMMC storage capabilities, and the NXP cores feature a 1.8 GHz quad-core Cortex-A53 MPU and a 400 MHz Corex-M4 microcontroller. The Nitrogen8M Mini SMARC can also function as a powerful single-board computer (SBC) on a standard SMARC carrier board to aid designers in simplifying their bill-of-materials (BOM) and getting their products to market faster.

For additional design flexibility, the Nitrogen8M Mini SMARC supports multiple connectivity interfaces, including two I2S audio interfaces, a MIPI-CSI camera interface, five I2C modules, PCIe, three USB2 interfaces, a GbE, SDIO/eMMC, two SPIs, UART and GPIO. The SOM is also regulatory compliant with global radio certifications, including FCC, ISED, CE, UKCA and more.

Ezurio's Nitrogen8M Mini SMARC is available now from Mouser Electronics in a SMARC 2.1.1 standard form factor of 82 mm x 50 mm and is offered in multiple high-performance memory options. Software support for the Nitrogen8M Mini SMARC includes Yocto Linux, Buildroot Linux, Android, Ubuntu, Zephyr RTOS and FreeRTOS. The SOM is specified at an industrial temperature range of -40°C to +85°C (commercial range of 0°C to +70°C), has a 10+ year product lifecycle, and is ideally suited for Smart buildings and appliances, industrial IoT (IIoT), HMI, touchscreens and displays, vision systems, food and beverage and medical devices.

To learn more, visit https://www.mouser.com/new/laird-connectivity/laird-connectivity-nitrogen8m-mini-smarc/.

 

Distributeur mondial agréé, Mouser dispose de la plus vaste sélection au monde de semi-conducteurs et composants électroniques à la pointe de la technologie, en stock et prêts à être expédiés. Les clients Mouser peuvent compter sur des produits d’origine entièrement certifiés dont la traçabilité de chacun de ses partenaires de fabrication est garantie. Afin d’accélérer le processus de conception des clients, le site Internet de Mouser propose une vaste bibliothèque comportant des ressources techniques, dont un centre de ressources techniques, ainsi que des fiches techniques, des conceptions de référence propres à des fournisseurs, des notes d’application, des informations sur des conceptions techniques, des outils d’ingénierie et bien d’autres informations pratiques.

À propos de Mouser

2026 - Mouser Electronics est un distributeur agréé de semi-conducteurs et de composants électroniques, spécialisé dans le lancement de nouveaux produits de ses partenaires de premier plan. Le site Internet du distributeur, Mouser.fr, est disponible en plusieurs langues et dans plusieurs devises, et propose plus de 6,8 millions de produits de plus de 1 200 marques de fabricants. Mouser dispose de 28 sites répartis dans le monde entier afin d’offrir à ses clients un service d’excellence dans la langue, la devise et le fuseau horaire du pays respectif. Le distributeur expédie ses produits à plus de 650 000 clients dans plus de 223 pays/territoires depuis son centre logistique de 93 000 m² de Dallas (Texas). Pour plus d'informations, rendez-vous sur https://www.mouser.fr.

About Ezurio

2026 - Ezurio turns design possibility into reality with a comprehensive range of RF modules, system-on-modules, single-board computers, internal antennas, IoT devices, and custom solutions. With decades of engineering expertise, Ezurio provides solutions that reduce development costs and time to market. Ezurio's global reach and unmatched support are backed by a resilient global supply chain that gives our customers the stability to overcome every design challenge with confidence. Turn design possibility into reality with Ezurio, your connectivity expert.

Laird Connectivity and Boundary Devices are now Ezurio.

Marques déposées

Mouser et Mouser Electronics sont des marques déposées de Mouser Electronics, Inc. Tous les autres produits, logos et noms de société cités dans le présent document, peuvent être des marques commerciales de leurs propriétaires respectifs.

Pour tout complément d'information, contactez :
Kevin Hess, Mouser Electronics
Vice-président senior responsable du marketing
+1 (817) 804-3833
Pour les questions liées à la presse, contactez :
Kelly DeGarmo, Mouser Electronics
Responsable de la communication institutionnelle et des relations avec les médias
+1 (817) 804-7764