Mouser Now Shipping ams OSRAM Mira220 Global Shutter Image Sensors for Machine Vision Applications

Annonce de nouveaux produits

Retrouvez-nous sur


February 15, 2023Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now shipping the Mira220 global shutter sensors from ams OSRAM. These sensors give design engineers 2D and 3D solutions for industrial machine vision applications like mobile facial authentication, smart home appliances, QR readers, AR/VR, drones, smart wearable devices, structured light vision and more.

The Mira220 2.2-megapixel global shutter image sensors support on-chip operations like external triggering, windowing, and both horizontal and vertical mirroring with an effective resolution of 1600 (H) x 1400 (V) at a maximum frame rate of 90 fps at 12-bit depth. The Mira220's advanced back-side illumination (BSI) technology stacks the sensor layer on top of the digital/readout layer. This design results in a chip-scale package with a footprint of just 5.3 mm × 5.3 mm, giving manufacturers greater freedom to optimize the design of space-constrained products such as smart glasses and VR headsets. The Mira220 also features very high sensitivity and quantum efficiency with a pixel size of 2.79 μm and is supplied in a 1/2.7” optical format.

The Mira220 features very low power consumption, with only 4 mW required in sleep mode, 40 mW in idle mode, and 350 mW at full resolution with  90 fps. By providing low system power consumption, the Mira220 enables wearable and portable device manufacturers to save space by specifying a smaller battery or extending run-time between charges. The ams OSRAM Mira220 sensors utilize the MIPI CSI-2® interface for easy interaction with processors and FPGAs, with on-chip registers that can be accessed via the standard I2C interface for easy sensor configuration. 

The ams OSRAM Mira220 global shutter image sensors are supported by the JetCis evaluation system, also available at Mouser. The JetCis evaluation system features an open development platform based on Linux running on the nVidia® Jetson Nano embedded system.

To learn more about the ams OSRAM Mira220 2.2MP global shutter image sensors, visit https://www.mouser.com/new/ams-osram/ams-osram-mira220-sensors/.

 

Distributeur mondial agréé, Mouser dispose de la plus vaste sélection au monde de semi-conducteurs et composants électroniques à la pointe de la technologie, en stock et prêts à être expédiés. Les clients Mouser peuvent compter sur des produits d’origine entièrement certifiés dont la traçabilité de chacun de ses partenaires de fabrication est garantie. Afin d’accélérer le processus de conception des clients, le site Internet de Mouser propose une vaste bibliothèque comportant des ressources techniques, dont un centre de ressources techniques, ainsi que des fiches techniques, des conceptions de référence propres à des fournisseurs, des notes d’application, des informations sur des conceptions techniques, des outils d’ingénierie et bien d’autres informations pratiques.

À propos de Mouser

2026 - Mouser Electronics est un distributeur agréé de semi-conducteurs et de composants électroniques, spécialisé dans le lancement de nouveaux produits de ses partenaires de premier plan. Le site Internet du distributeur, Mouser.fr, est disponible en plusieurs langues et dans plusieurs devises, et propose plus de 6,8 millions de produits de plus de 1 200 marques de fabricants. Mouser dispose de 28 sites répartis dans le monde entier afin d’offrir à ses clients un service d’excellence dans la langue, la devise et le fuseau horaire du pays respectif. Le distributeur expédie ses produits à plus de 650 000 clients dans plus de 223 pays/territoires depuis son centre logistique de 93 000 m² de Dallas (Texas). Pour plus d'informations, rendez-vous sur https://www.mouser.fr.

À propos de ams OSRAM

2026 - Le groupe Ams OSRAM est un leader mondial dans le domaine des capteurs et émetteurs intelligents. L'entreprise se concentre sur l'innovation dans les domaines de la détection, de l'éclairage et de la visualisation afin de rendre les trajets plus sûrs, les diagnostics médicaux plus précis et les moments de communication quotidiens plus riches en expériences. Avec plus de 110 années d'histoire combinée, le cœur de ams OSRAM est défini par l'imagination, une expertise approfondie en ingénierie et la capacité à fournir une capacité industrielle mondiale dans capteur et les technologies légères. ams OSRAM crée une technologie pour des applications révolutionnaires, ce qui se reflète dans plus de 15 000 brevets accordés et déposés. En ajoutant de l'intelligence à la lumière et de la passion à l'innovation, ams OSRAM enrichit la vie des gens.

Marques déposées

Mouser et Mouser Electronics sont des marques déposées de Mouser Electronics, Inc. Tous les autres produits, logos et noms de société cités dans le présent document, peuvent être des marques commerciales de leurs propriétaires respectifs.

Pour tout complément d'information, contactez :
Kevin Hess, Mouser Electronics
Vice-président senior responsable du marketing
+1 (817) 804-3833
Pour les questions liées à la presse, contactez :
Kelly DeGarmo, Mouser Electronics
Responsable de la communication institutionnelle et des relations avec les médias
+1 (817) 804-7764