Renesas Electronics' RA8P1 Microcontrollers, Now at Mouser, Deliver High CPU Performance for Advanced Artificial Intelligence
September 2, 2025 – Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the RA8P1 Microcontrollers (MCUs) from Renesas Electronics. The RA8P1 Microcontrollers combine Arm® Cortex®-M85 (CM85) and Cortex-M33 (CM33) central processing unit (CPU) cores with the Arm Ethos-U55 micro neural processing unit (µNPU) to deliver superior CPU and AI (Artificial Intelligence) performance. The RA8P1 MCUs are optimized for edge and Internet of Things (IoT) applications, including robotics, security cameras, home appliances, and voice and vision AI.
The Renesas Electronics RA8P1 Microcontrollers, now available at Mouser, deliver CPU performance of over 7,300 CoreMarks and AI performance of 256 giga operations per second (GOPS) at 500 MHz. Advanced AI capabilities enable voice AI (KWS, ASR, and NLP), vision AI (object detection, image classification, and face recognition), and real-time analytics (vibration analysis and anomaly detection) on a single chip. Further features include large memory, multiple external memory interfaces, and an advanced peripheral set optimized for AI applications. The RA8P1 MCUs are built on the advanced 22nm ultra-low leakage (ULL) process for ultra-high performance with very low power consumption. The RA8P1 is available as a single-core MCU and dual-core MCU with an embedded Cortex-M33 core. Delivered in 224 and 289 BGA packages, the RA8P1 MCUs are ideal for a range of uses across markets. The RA8P1 MCUs provide security for critical applications through an advanced cryptographic security IP, immutable storage, tamper protection, and Arm TrustZone®.
The Renesas Electronics EK-RA8P1 Evaluation Kit, also available at Mouser, allows users to easily evaluate the RA8P1 MCU microcontrollers. The kit provides all the features and interface options required to streamline and accelerate the evaluation process.
To learn more about the RA8P1 MCUs, visit https://www.mouser.com/new/renesas/renesas-ra8p1-mcus/.
For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.
Distributeur mondial agréé, Mouser dispose de la plus vaste sélection au monde de semi-conducteurs et composants électroniques à la pointe de la technologie, en stock et prêts à être expédiés. Les clients Mouser peuvent compter sur des produits d’origine entièrement certifiés dont la traçabilité de chacun de ses partenaires de fabrication est garantie. Afin d’accélérer le processus de conception des clients, le site Internet de Mouser propose une vaste bibliothèque comportant des ressources techniques, dont un centre de ressources techniques, ainsi que des fiches techniques, des conceptions de référence propres à des fournisseurs, des notes d’application, des informations sur des conceptions techniques, des outils d’ingénierie et bien d’autres informations pratiques.
2026 - Mouser Electronics est un distributeur agréé de semi-conducteurs et de composants électroniques, spécialisé dans le lancement de nouveaux produits de ses partenaires de premier plan. Le site Internet du distributeur, Mouser.fr, est disponible en plusieurs langues et dans plusieurs devises, et propose plus de 6,8 millions de produits de plus de 1 200 marques de fabricants. Mouser dispose de 28 sites répartis dans le monde entier afin d’offrir à ses clients un service d’excellence dans la langue, la devise et le fuseau horaire du pays respectif. Le distributeur expédie ses produits à plus de 650 000 clients dans plus de 223 pays/territoires depuis son centre logistique de 93 000 m² de Dallas (Texas). Pour plus d'informations, rendez-vous sur https://www.mouser.fr.
Mouser et Mouser Electronics sont des marques déposées de Mouser Electronics, Inc. Tous les autres produits, logos et noms de société cités dans le présent document, peuvent être des marques commerciales de leurs propriétaires respectifs.